Final Steps
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Cleaning the panel and checking panel assembly
| NOTICE |
|---|
|
HAZARD OF Incorrect Cleaning and Checking of Assembly
Observe the following instructions for this step.
Failure to follow these instructions can result in equipment damage.
|
-
Clean the switchgear, removing contamination resulting from assembly work.
-
Remove all the attached information tags, cards, brochures and instructions no longer needed.
-
Check the tightening torques of all screw fastenings and connections established on the site of installation:
-
High-voltage connection
-
Earth conductor
-
Panel screw fastenings
-
Busbar links
-
Special attachments.
-
Damaged paint
The panels are powder-coated. Minor damage to the paint can be repaired using commercially available paint (standard colour RAL 7044 or corresponding colour).
Re-mounting the covers
-
Removed partition and cover plates in the busbar and switching device compartment (see Front Access)
-
Cable duct covers of the external control and measurement cables.
-
Cable compartment cover (see Access to the Cable Compartment).
-
Remove temporary base from the panel top, if such a base has been used(see Top Access).
Inspection
-
Check the switchgear for damage which might be due to transport or assembly work.
-
Compare data on nameplate to the required ratings.
Racking-in the trucks
Insert trucks in the panels depending on the panel configuration (see Inserting the Circuit Breaker into the Panel):
-
Disconnector truck EvoPact UTX
-
Vacuum contactor CVX
-
Metering truck EvoPact MTX
-
Circuit breaker truck EvoPact HVX
Close front doors
For details, refer to Opening and Closing the Front Door.
DANGER