GEX2564100SWE-00(NORDICS)

Safety Provisions

After removal of covers, isolate the appropriate part of the switchgear unit from the power supply, for the operator safety in accordance to IEC 62271-200.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Before opening, removing doors or covers, isolate the compartment in question.
  • Check for zero voltage and earth in accordance with the safety provisions in EN 50110-1.
Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?