GEX2564100SWE-00(NORDICS)

Description of VDIS Unit

The VDIS unit is a self-powered voltage detecting and indicating system.

The VDIS unit is integrated into Schneider Electric cubicles, flush-mountable and designed according to standard IEC 62271-213: 2021. The VDIS unit is fitted with a three LED display and detects the operating voltage presence/absence on the Cubicle main unit.

NOTE: VDIS is not used to distinguish between voltage not present (that is U <10 % of nominal voltage) and dead circuit state (that is U = 0 V).

When installing the VDIS into the cubicle the fixation screws are required to be tightened to between 0.6 N•m and 1 N•m. When fixing the coupling sub-assembly to the Indication sub-assembly the screws are required to be tightened to between 0.6 N•m and 1 N•m. Check that the seal between the coupling and indication sub-assemblies completely covers the coupling sub-assembly before fixing the two sub-assemblies together.

Check that the seal fits flush between the two sub-assemblies and is not twisted or creased.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?