GEX2564100SWE-00(NORDICS)

Shipping Units

  • The conditions and types of transport have been stipulated in the contract details.

  • The type of packaging depends on the type of transport and the storage conditions.

  • The panels are delivered individually and are fastened on pallets. The standard accessories are included.

  • In the case of panels with a width of 650, 750 and 800 mm, the trucks can be delivered within the panels. They are in disconnected position. With 1000 mm wide panels, the trucks are delivered in separate packaging.

  • The panels are delivered in vertical position.

  • The weight of the entire transport unit is indicated on the packaging.

Packaging

  • If packed exclusively for truck transport, the panels are delivered on a pallet with PE protective film (Figure 17).

  • For sea transport, the units are packed in sealed aluminium foil with desiccant and in a closed wooden case with tightly closed wooden base (also for container transport, see Figure 18).

  • In case of air transport, the panels are packed in wooden crates with a protective PE film hood (dust protection) or in wooden crates, also with closed wooden bases, however without protective hoods (Figure 18).

When transporting the switchgear panels, check that the transport units do not shift or tilt over (nail the transport pallet to the loading bed if necessary). Observe the centre of gravity label (see Figure 18) to help ensure safe transport. You can find the label on the packaging or on the switchgear panel.

Figure 17
Packaging in PE protective film, on a pallet

Figure 18
Centre of gravity information on the transport unit (wooden crate for export packaging)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?