GEX2564100SWE-00(NORDICS)

Storage

WARNING
HAZARD OF INCORRECT STORAGE
Sufficient stability and evenness of the supporting area must be ensured.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

If the panels are not installed immediately after delivery, they can be stored under the following conditions:

  • Panels should be stored in vertical positions and should not be stacked.

  • Indoor storage only is admissible.

  • Switchgear and accessories should be stored sealed with desiccants in aluminum foil and packed in a wooden box (the storing time before installation is compliant with the warranty period in the terms and conditions).

  • Pallet should not be removed until the installation.

  • Storage only in packed condition. Performance will not be guaranteed if stored in open condition.

  • The storage room environment should be healthy, no rodents, humidity control ≤95%/≤90% for 24 hrs and 1 month respectively, and no water on the floor.

Figure 23
Schematic diagram of the storage conditions for PIX panels

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?