GEX2564100SWE-00(NORDICS)

Feeder Panels with Switching Devices

 

Figure 4
Feeder panel with circuit breaker truck EvoPact HVX for rated currents > 2500 A and voltage transformer (optional)

 

Figure 5
Feeder panel with circuit breaker truck EvoPact HVX for rated currents ≤ 2500 A and voltage transformer (optional)

 

Figure 6
Panel with disconnector truck EvoPact UTX

 

Figure 7
Motor Control Center panel with vacuum contactor CVX (only 12 kV)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?