Transport
WARNING |
|---|
|
hazard of TOPPLING
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Transport with Forklift Truck
CAUTION |
|---|
|
HAZARD OF DEVICE FALLING
Failure to follow these instructions can result in injury or equipment damage.
|
Transport with circuit breaker in the switchgear panel (for 650, 750 and 800 mm panel width)
Delivery takes place in the position:
-
Circuit breaker in the test position
-
Earthing switch ON
Delivery
| NOTICE |
|---|
|
hazard of INADEQUATE HANDLING
Handle shipping units carefully when unloading and unpacking
them.
Failure to follow these instructions can result in equipment damage.
|
Shipping units must be checked upon receipt. Any damage which may have occurred in transit must be recorded and reported to the manufacturer immediately.
Check completeness of consignment based on the transport documents.
The supplier must be notified in writing without delay about any deviations.
WARNING
CAUTION