Requirements Regarding the Switchgear Room
Before installing the switchgear panels:
-
Refer and comply with the switchgear room measurements mentioned in the document.
-
Observe the minimum distance between the switchgear and the wall of the building.
-
The load-bearing capacity of the fastening areas must correspond to the weight of the switchgear (perform a stress analysis of the building).
-
Check base frame (if used) for dimensions and positional tolerances.
-
Check position of floor openings for high-voltage and low-voltage cables.
Before the switchgear is positioned at its site of installation, check that the fastening points are level. Unevenness must not exceed ± 2 mm/meter and 6 mm difference in height over the entire switchgear width.
|
Basic structure panels |
Pressure relief |
|||||
|---|---|---|---|---|---|---|
|
Outside the building only |
||||||
|
Tunnel |
||||||
|
Ur |
H |
LV |
H3 |
T |
H1 |
H2 |
|
12 kV |
2130 |
530 |
2130 |
330 |
290 |
2750 |
|
630 |
2230 |
|||||
|
730 |
2330 |
|||||
|
17 kV |
2200 |
600 |
2200 |
330 |
220 |
2750 |
|
700 |
2300 |
|||||
|
800 |
2400 |
|||||
|
24 kV |
2330 |
530 |
2330 |
330 |
90 |
2750 |
|
630 |
2430 |
|||||
|
730 |
2530 |
|||||
| H |
Panel height, basic structure |
|||||
|
LV |
LV box height |
|||||
|
H3 |
Basic panel including LV box height |
|||||
|
T |
Tunnel height |
|||||
|
H1 |
Distance to ceiling |
|||||
|
H2 |
Height of ceiling |
|||||
|
Tunnel |
||||||
|
R |
Distance to rear wall |
>100 mm |
||||
|
D |
Width of control aisle |
1500 mm |
||||
|
Panel replacement |
2000 mm |
|||||
|
(1) With standard LV cabinet 530 mm. Increased height of LV cabinet is available, without impact on the ceiling height. |
||||||
|
(2) Height of 30mm for AVVS is considered. |
||||||
|
(3) Minimum 90 mm. |
||||||
Ground Plan of a PIX Switchgear within a Switchgear Room
Figure 39
Design example: The switchgear
is located in the left-hand corner of the room
|
1 |
Bore-hole for fastening of panel |
|
2 |
Switchgear side wall |
|
3 |
Openings for routing external low-voltage cables |
|
4 |
Openings for routing high-voltage cables |
|
5 |
Reserved (100 x 100 mm) for the connection of the earth bus of the switchgear to the building’s earth cable |