GEX2564100SWE-00(NORDICS)

Removing the Transport Lock of the Circuit Breaker

In the case of panels with a width of 650, 750 and 800 mm, the circuit breakers can be delivered within the panels and transport locks (Figure 28) that helps to secure the circuit breaker.

Follow the below steps to remove the transport lock of the circuit breaker

  1. Release the two bolts (Figure 29, 1).

  2. Release lock bolts M8 x 25 (2).

  3. Remove transport lock (3).

  4. Reinsert the two bolts (1).

Remove transport lock on the other side following the same procedure.

Figure 28
Transport lock of circuit-breaker truck

Figure 29
Remove transport lock

1 Bolts
2 Lock bolts
3 Transport lock

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?