GEX2564100SWE-00(NORDICS)

Removing the Cable Compartment Cover

Follow the below steps to remove the cable compartment cover:

  1. Release the securing bolts of the cable compartment cover as shown in (Figure 24, 1).

  2. Lift and remove the cable compartment cover (2).

    Figure 24
    Transport units must not tip over

    1

    Securing bolts

    2

    Compartment cover

Re-mounting the Cable Compartment Cover

After terminating assembly work, place cable compartment cover onto the panel and lower it till the arrow sticker of cable matches with the arrow sticker of panel.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?