GEX2564100SWE-00(NORDICS)

Front Access

Follow the below steps to access the busbar compartment from front side:

  1. Remove cable compartment cover (Figure 37, 1).

  2. Open front door (see Opening and Closing the Front Door).

  3. Remove circuit breaker EvoPact HVX, UTX etc. (see Removing the Circuit Breaker from the Panel).

  4. Remove circuit breaker(see Access to the Cable Compartment).

  5. Unscrew pressure relief flap (5) and take it out in forward direction.

  6. Remove partition plate (6) to busbar compartment and take it out in forward direction.

  7. Insert temporary base plate (7) to enable safe access to the cable compartment.

Figure 37

1 Remove cable compartment cover
2 Open front door
3 Remove circuit breaker (the example shows the circuit breaker truck EvoPact HVX)
4 Remove truck carrier
5 Unscrew pressure relief flap and take it out in forward direction
6 Remove partition plate to busbar compartment and take it out in forward direction
7 Insert temporary base plate to enable safe access to the cable compartment
8 Busbar compartment
9 Working position
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?