GEX2564100SWE-00(NORDICS)

List of the Assembly Drawings

List of all assembly drawings specified in this manual. This does not apply to special modules or customer-specific special designs.

According to the switchgear configuration in question, only such drawings from the list are supplied by the factory as are actually required.

Description

Assembly drawing Chapter

Chapter

Panel fastening on concrete foundations

SEM102173-01

5.5

Screw-fastening the panels to one another

SEM102056-01

5.7

Mounting the low-voltage compartments

AGS C73 180-01

7.2

Mounting an additional cable duct

AMT 000 376-01

7.4.2

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?