Technical Data of Electrical Control and Operating Devices
The switchgear panels have been designed on principle so as to permit manual operation.
The drive mechanisms of the individual switching devices can be equipped, depending on the specific customer‘s model, with additional electrical control and operating devices. These are defined in the switchgear-specific circuit diagram (see switchgear documentation).
Component fitting options:
-
Motor-operated drive mechanism for the earthing switch control element
-
Blocking coil
The blocking coil helps to prevent manual actuation of the earthing switch. If the supply voltage has failed or is shut off, all blocking coils are in blocked position.
-
Auxiliary switches
Auxiliary switches are always actuated directly by the truck or by the switch shaft via an intermediate linkage. Their position always corresponds to that of the main contacts. The switching functions have been set in the factory according to the circuit diagram.
-
Micro-switches are used depending on the customized panel models.
Overview of rated supply voltages
|
Overview of rated supply voltages |
||||||
|---|---|---|---|---|---|---|
|
Direct voltage DC |
24 V |
48 V |
60 V |
110 V |
125 V |
220 V |
|
Alternating voltage AC |
(110)/120 V |
(220)/230 V |
||||
Power consumption
|
Device |
Rated power consumption |
|
|---|---|---|
|
DC approx. [W] |
AC 50/60 Hz approx. [VA] |
|
|
Blocking coil |
12 |
|
|
Motor for earthing switch |
150 |
|
Information about the power consumption of solenoids and the motor is available in the related user guides, for example EvoPact HVX and CVX.
Trucks
Electrical control and operating devices of trucks are described in the appropriate Technical Manuals (see Reference documents)
-
Circuit breaker EvoPact HVX with 12–24 kV, Ir ≤ 2500 A see Technical Instruction AGS 531301-01
-
Disconnector truck EvoPact UTX/Metering truck EvoPact MTX up to 24 kV see Technical Instruction AGS 531361-01
-
Vacuum contactor CVX see Technical Instruction NTV 133