GEX2564100SWE-00(NORDICS)

Transport on the Floor

Follow the below steps to transport the panels and circuit breakers using cylindrical rollers:

  1. Push panel onto three cylindrical rollers (minimum diameter 30 mm)

    (Figure 43).

  2. Move the panel until it reaches its final location.

Figure 43
Transport of the panel on the floor

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?