Transport Trolley for Circuit Breaker
|
1 |
Autonomous interlocking of the racked-in truck on the trolley |
|
2 |
Variable screw fastening of track |
|
3 |
Positioning of track to adjust the various track widths |
|
4 |
Track |
|
5 |
Interlocking with panel |
|
6 |
Variable screw fastening of unlocking bar |
|
7 |
Positioning of unlocking bar to match various panel versions |
|
8 |
Tray for accessories (lever, keys, handle) |
|
9 |
Lever to lock / unlock the transport trolley on the panel. Table of trolley is lifted or lowered. |
|
10 |
Unlocking bar. The truck is unlocked in the panel. |
|
11 |
Handles of trolley |
|
12 |
Slide to unlock the truck from the trolley |
|
Rated volt-age Ur of the panel [kV] |
Panel width [mm] |
Truck |
Item number of trolley |
|
≤ 12 |
650/800 |
EvoPact HVX / UTX / MTX and CVX |
EIB AE1 148-01(1) |
|
1000 |
EvoPact HVX / UTX (Ir = 2500 A) |
EIB AE1 148-02 |
|
|
EvoPact HVX / UTX (Ir = 3150 A) |
AGS C74 125-01 |
||
|
≤ 17.5 |
750 |
EvoPact HVX / UTX / MTX and CVX |
EIB AE1 148-01(1) |
|
1000 |
EvoPact HVX / UTX (Ir = 2500 A) |
EIB AE1 148-02 |
|
|
EvoPact HVX / UTX (Ir = 3150 A) |
AGS C74 125-01(1) |
||
|
24 |
800 |
EvoPact HVX / UTX / MTX and CVX |
EIB AE1 148-01(1) |
|
1000 |
EvoPact HVX / UTX (Ir = 2500 A) |
EIB AE1 148-02 |
|
|
(1) The trolley can be used for panel widths of 650, 750 and 800 mm. |
|||
Adjusting the track width
Follow the steps to adjusting the track width:
-
Release 3 screws on each track (Figure 80, 2).
-
Adjust the two tracks to the appropriate panel track width and check them. Remount the six screws.
-
Adapt position of unlocking bar (10) also to the appropriate panel (same procedure).