GEX2564100SWE-00(NORDICS)

Transport using a Crane

Follow the below steps to transport the panels and circuit breakers using crane:

  1. Attach the crane straps in the four jack rings on top of the panel (Figure 41), maintaining a minimum height of 1 m (Figure 42).

  2. Release the front and rear panel screw fastening from the transport packaging. To this effect, remove the cable compartment cover, see Opening and Closing the Front Door.

  3. Carefully lift the panel and deposit it at the intended location.

Figure 41
Jack rings on top of the panel

Figure 42
Observe the minimum height

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?