About the Document
Intended Use
This Installation Manual describes air-insulated medium-voltage switchgear units of the series PIX Sweden.
It is exclusively intended for use by the manufacturer's staff or by persons certified for the PIX series (training certificate).
Read instructions before operating, servicing, or doing maintenance of the equipment.
This Installation Manual is an integral part of the product and should be stored so that it is readily accessible at all times for and can be used by persons who are to work on the switchgear. If the switchgear is relocated to another site, this Installation Manual must be passed on to the new operators along with the unit.
As our products are subject to continuous development; we reserve the right to make changes regarding the standards, illustrations and technical data described in this Installation Manual.
This Installation Manual cannot describe every imaginable individual case or every customer-specific version of the product. For information which is not included in this manual, contact the manufacturer.
All dimensional data in this manual is in millimetres.
Related Documents
The following additional documents must be complied with:
-
Purchase agreement with the stipulations regarding the switchgear-specific equipment and the legal details
-
The appropriate switchgear-specific circuit diagrams/documentation
-
The operating manuals of the low-voltage devices installed in the switchgear (for example, voltage presence detecting systems and devices in low-voltage cabinet)
-
The assembly drawings supplied with the equipment
-
The assembly instructions of the manufacturer of the cable connection systems to be connected to the switchgear
-
The operating instructions of the trucks being used
|
Title of Document |
Reference Number |
|---|---|
|
EvoPact HVX Vacuum Circuit Breaker 12–24 kV, Ir ≤ 2500 A |
AGS531301-01 |
|
Metering Truck EvoPact MTX and Disconnector Truck EvoPact UTX up to 24 kV |
AGS 531361-01 |
|
Vacuum Contactor CVX |
NTV 133 |
|
Voltage Transformer Truck in Cable Compartment (can be Racked Out) |
AGS 531505-02 |
|
PIX Additional Equipment |
AMTNoT 077-02 |
|
Motor Control Center with Ur ≤ 7.2 kV |
AGS 531500-02 |