GEX2564100SWE-00(NORDICS)

Circuit Breakers

The circuit breakers can be transported by means of the optional handling crane (Figure 44).

Verify the circuit breakers are always placed on external wooden beams (Figure 45).

Figure 44
Transport of circuit breaker using the handling crane

Figure 45
Circuit breakers must always be placed on external wooden beams

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?