GEX2564100SWE-00(NORDICS)

Installation of the Busbar Bushings

Panels can be equipped, depending on the customer specifications, with retaining plates to increase the mechanical strength (Figure 50 and Figure 51) or busbar section segregations to increase the mechanical strength (Figure 49).

The Busbar retaining plate (1), Busbar section segregation and the bushings (2) with retaining ring and rubber part are included in the accessories.

Slip bushing from the outside through the bore-hole and mount retaining ring from the inside.

Figure 49

1 Busbar section segregation (option)

2 Bushing

Figure 50

1 Busbar retaining plate

2 Bushing

3 Retaining ring

Figure 51
Busbar retaining plate in bus section couplers

 
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?