GEX2564100SWE-00(NORDICS)

Routing the External Cables through an Additional Cable Duct (Optional)

Customized low-voltage cables for control and measurement can be routed via an optional, separate cable duct above the low-voltage compartment (Figure 70).

The cable duct is mounted on site, and is included in the accessories.

  1. Mount the cable duct in accordance with the assembly drawing AMT 000 376- 01.

  2. Route external cables through the cable duct (2) to the lowvoltage compartment (3). Connect external cables to the terminal strips in the low-voltage compartment according to the circuit diagram.

  3. Screw-fasten cover of cable duct (1).

Figure 70
Top cable duct

1 Cable duct cover

2 Cable duct

3 Low-voltage compartment

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?