GEX2564100SWE-00(NORDICS)

Connection of the Ring Circuits in the Low-Voltage Compartment

Follow the below steps to connect of the ring circuits in the low-voltage compartment.

  1. Route the ring circuits for the intra-panel wiring through the lateral openings of the low-voltage compartment (Figure 68, 2).

  2. The ring circuits have been designed with connectors. Connect ring circuits in accordance with the connector identification (or the circuit diagram) to the appropriate terminal strips in the low-voltage compartment.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?