GEX2564100SWE-00(NORDICS)

Safety Provisions

The switchgear panels may only be installed and assembled by the manufacturer’s staff or by persons who have been certified for this work.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
During assembly, installation and connection, the energy storing devices must not be charged.
Failure to follow these instructions will result in death or serious injury.
WARNING
hazard of incorrect operation
  • Watch out for floor openings in the switchgear room.
  • Do not walk on the top sides of the panels. When work has to be performed on the panel top, for example for assembly of fans or pressure relief ducts, temporarily position a solid base plate to step on.
  • The switchgear panels must only be installed and assembled by the manufacturer’s staff or by persons who have been certified for this work.
  • Observe the safety provisions.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?