GEX2564100SWE-00(NORDICS)

Top Access

WARNING
hazard of FALLING
  • Do not walk upon the topsides of the switchgear cubicles.
  • During civil engineering activities, when working on the top of the switchgear cubicles (such as during the installation of deflectors, fans, or pressure relief ducts), temporarily attach a sturdy base plate that is walkable.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Access to the busbar is possible from the top as well (Figure 38) provided the space available so permits (sufficient ceiling height is required).

  1. Cover top of panel using a temporary base plate (1).

  2. Release the screw fastening of the upper busbar compartment cover (2) and remove sheet metal cover (3). Now, the busbar compartment (4) is accessible.

Figure 38
Top access to the busbar compartment

1 Temporary base plate

2 Screw fastening

3 Sheet metal cover

4 Busbar compartment

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?