GEX2564100SWE-00(NORDICS)

Important Information for Assembly

PIX panels are delivered with the earthing switch ON.

In the case of panels with a width of 800 mm, the trucks can be delivered within the panels. They are in disconnected position. The circuit breakers are always shipped in open state (OFF) with the energy storing device released.

CAUTION
hazard of incorrect assembly
  • Condensation, dirt and dust during assembly must be avoided on all accounts, in order to prevent damage to the panels.
  • For assembly, observe the assembly drawings supplied with the equipment.
  • For all Screw Fastenings, comply with the tightening torques specified.
Failure to follow these instructions can result in injury or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?