GEX2564100SWE-00(NORDICS)

Screw-fastening the Panels to One Another

Assembly drawing: SEM102056-01.

Follow the below steps to screw fastening the panels to one another:

  1. Screw-fastening panel fronts to one another using 6 fastening points (Figure 48).

  2. Fasten panels to one another at the top on the rear side using a connecting link. To this effect, use the screws provided on the panel.

Figure 48
Screw-fastening the panels to one another

1

Screw M8

2

Spring washer

3

Hex. nut M8 with lock washer

4

Connecting link

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?