GEX2564100SWE-00(NORDICS)

Inserting the Circuit Breaker into the Panel

NOTICE
HAZARD OF ABNORMAL USE CONDITIONS
Circuit breakers and panels must match rating to prevent the truck from being racked completely into the panel.
Failure to follow these instructions can result in equipment damage.

Follow the below steps to insert the circuit breaker into the panel:

  1. Move the circuit breaker on the trolley in front of the panel.

  2. Turn the lever on the trolley clockwise to lift the transport table.

  3. Move the trolley on the handles (2) with the lateral guides (3) to the panel and turn the lever to the right again.

  4. Press the left release button (Figure 36, 5) and push the circuit breaker briefly over the locking lever.

  5. Push the circuit breaker into the panel by means of the handles (6) until it engages in the control panel.

  6. Turn the lever to the left again (7).

    The trolley is lifted at the front and released from the panel.

  7. Pull the trolley away from the panel and turn the lever to the right again to lower it.

Figure 35
Move trolley with circuit breaker towards the panel until they are in contact, and lock.

Figure 36
Pushing the circuit breaker into the panel.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?