Cable Test after Assembly
WARNING |
|---|
|
hazard of incorrect operation
Comply with the safety provisions.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
A test unit and a test adapter (not included in scope of supply) are required for cable testing.
During the cable test, the busbar can be operated at rated voltage (see nameplate). For qualification of the current transformers for cable tests, enquire at the appropriate manufacturer's.
Preparation
WARNING |
|---|
|
hazard of incorrect operation
Strictly observe the assembly instructions for the test
adapters and the operating and inspection instructions for the test
unit.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
-
Isolate outgoing feeder cable of the panel to be tested.
-
Isolate outgoing feeder cable in remote station.
-
Earth outgoing feeder cable of the panel to be tested.
-
Remove cable compartment cover (see Access to the Cable Compartment).
-
Disconnect voltage transformer and surge arrester; earth voltage detecting systems.
Performing the cable test
-
Connect the test adapter to a free cable connection in the panel and on the test unit. To this effect, observe the specifications of the test unit’s manufacturer.
-
Set switchgear panel to test position:
Circuit breaker OFF Truck In disconnected position Earthing switch OFF -
Perform cable test according to the cable manufacturer’s specifications. When doing so, do not exceed the admissible limits (see Table).
Once the cable test has been completed:
-
Earth feeder cable again.
-
Remove test set.
-
Reconnect voltage transformer, surge arrester and voltage detection systems or de-earth them.
-
Reposition cable compartment cover.
Admissible limits for the cable test in panels
| Admissible limits for the cable test in panels(1) |
DC test voltage [kV] max. 15 min. |
|---|---|
|
PIX 12 |
34 |
|
PIX 17 |
42 |
|
PIX 24 |
67 |
(1) Admissible limits for the switchgear in case of cable tests with a testing frequency of 0.1 Hz available on request from the manufacturer’s.
WARNING