VDRB05981-03

Cubicle Design

PIX-36 Cubicle with HVX-O Circuit Breaker

1

Low-voltage cabinet with control devices

11

Current transformers

2

Metallic shutter for bus side

12

Earthing switch

3

Spout

13

Cable connections

4

CB compartment

14

Phase barriers

5

CB HVX-O

15

Rear cover

6

Metallic shutter of cable side

16

Cable compartment

7

Guide rails

17

Base frame

8

Front door

18

Cable clamp assembly

9

Busbar compartment

19

Earth bus

10

Risers

20

Pressure relief flaps

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?