VDRB05981-03

Safety Provisions for Installation

DANGER
hazard of Electric shock, explosion, or arc flash
During assembly, installation, and connection, the energy-storing devices must not be charged.
Failure to follow these instructions will result in death or serious injury.
WARNING
hazard of toppling
When handling the moving devices, pay attention to uneven floor surfaces (for example, cracks, projections, and so on) of the switchgear room.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
WARNING
HAZARD OF FALLING
  • Do not walk upon the topsides of the switchgear cubicles.
  • During civil engineering activities, when working on the top of the switchgear panels (such as during the installation of deflectors, fans, or pressure relief ducts), temporarily attach a sturdy and walkable base plate.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
WARNING
hazard of incorrect Installation
  • The switchgear cubicles must only be installed and assembled by the manufacturer’s staff or by persons who are certified for this work.
  • Observe the Safety Provisions.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?