VDRB05981-03

Low-voltage Connection

Connection to the ring circuits in the low-voltage cabinet

Follow the below steps to connect the ring circuits:

  1. Route the ring circuits for the inter-panel wiring through the lateral openings of the low-voltage cabinet.

  2. Connect ring circuits to the appropriate terminal strips in the low-voltage cabinet according to the circuit diagram.

Connection of low-voltage cable

1

Terminal strip

2

Openings for ring circuits in the low-voltage cabinet

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?