VDRB05981-03

Switching the Earthing Switch Manually

WARNING
hazard of inappropriate operation
  • Do not attempt to rack-in the breaker if earthing switch is ON.
  • Do not attempt to close the earthing switch if the circuit breaker is in service position.
  • Do not attempt to force open the flap, ensure circuit breaker is in test position.
  • Do not forcibly rack-in circuit breaker, ensure earthing switch is OFF and the flap is completely closed.
  • Do not release the push button after inserting the handle and before earthing switch is closed (in case of solenoid interlock).
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Follow the below Earth switch operating sequence, in case of non-compliance will complaint of earth switch interlock failure. Please contact Schneider Electric for further details.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?