VDRB05981-03

Switching OFF the Earthing Switch

Initial Situation:

  • Earthing switch: ON

  • Circuit Breaker: OFF

  • Truck: Disconnected position

Follow the below steps to switch OFF the earthing switch:

  1. Rotate the flap anti-clockwise to access the operating shaft.

  2. Insert operating handle aligned with axis point.

  3. Turn the handle clockwise by the 90°.

  4. Check the earthing switch position indicator through cable compartment inspection window and ensure that the earthing switch is OFF.

  5. Remove the earthing switch handle and place it back into the tool board.

  6. Close the flap completely (clockwise).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?