VDRB05981-03

Operating the EvoPacT HVX-O

Operator Interface

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR BURN
  • Installation, repair, and maintenance work on the EvoPacT HVX-O must only be carried out by qualified and certified personnel.
  • Beware of potential danger, apply appropriate PPE.
  • Follow safe electrical work practices.
Failure to follow these instructions will result in death or serious injury.

Operator interface of HVX-O

1

OFF button (rocker “O”) or push button “O”

2

ON button (rocker “I”) or push button “I ”

3

Operations counter

4

Rating plate

5

Position indicator of EvoPacT HVX-O

6

Position indicator of closing spring

7

Insertion opening for charging the closing spring

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?