VDRB05981-03

Switching a Feeder Cable

Initial Situation:

  • Circuit Breaker: OFF

  • EvoPacT HVX-O: Disconnected/test position

  • Earthing switch: OFF

Switch Feeder Cable ON


Switch Feeder Cable ON

Follow the below steps to switch outgoing feeder cable ON:

  1. Move the truck into connected/service position (1).

  2. Switch ON the circuit breaker (2).

Switch Feeder Cable OFF

Follow the below steps to switch outgoing feeder cable OFF:

  1. Switch OFF the circuit breaker.

  2. Move the truck into disconnected/test position.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?