VDRB05981-03

Operating Specifications

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
  • The switchgear unit may only be operated by specialist electricians who have proven experience (training certificate) in conjunction with the PIX-36 series and all relevant safety provisions.
  • Comply with the operating sequences described below.
  • Perform every switching operation completely.
Failure to follow these instructions will result in death or serious injury.
NOTICE
HAZARD OF INAPPROPRIATE OPERATION
  • While the power supply is not available, blocking coils (locking the interrogation slides and circuit-breaker push-buttons, depending on design), are in “locked” position. An under voltage release (optional) has dropped out.
  • Measure: Re-establish the supply voltage.
  • After each switching operation for which you have used a crank or a lever, remove this tool and store it in the tool board.
Failure to follow these instructions can result in equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?