VDRB05981-03

PIX-36 Switchgear Cubicle Ratings

Switchgear Cubicle kV Value

Rated voltage

Ur

kV

36

Rated lightening impulse withstand voltage

Up

kV

170

Rated power frequency withstand voltage

Ud

kV

70

Rated frequency

fr

Hz

50

Rated normal current

Ir

A

800

1250

2000

2500(1)

3150(1)

Rated short-time circuit

Ik

kA

26.3 (3 s) / 65.75

Rated peak withstand current

Ip

kA

31.5 (3 s) / 78.75

Internal arc classification (IAC AFLR)

-

kA

31.5 (0.1 s)

31.5 (1 s)

(!) Force cooling

The short-circuit capability of the current transformers must be considered separately.
NOTE:
  • The applicable panel-specific technical data are indicated on the Rating Plate (refer to Nameplate) and in the switchgear-specific documentation.

  • The technical data of the switching device (HVX-O, UTX-O, ETX-O) are indicated on the nameplate and in the operating manual of the device concerned.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?