Operating Interface of the Cubicle
|
1 |
Feeder Nameplate |
9 |
Insertion opening for racking the truck in/out manually |
|
2 |
Rating plate |
10 |
Slide for opening the insertion opening (9) for racking the truck in and out |
|
3 |
Handle for pulling door |
11 |
Window for checking Test / Service indication |
|
4 |
Operating handle for door locking and unlocking |
12 |
Low-voltage cabinet with control unit |
|
5 |
Switching EvoPacT HVX-O ON |
13 |
Handle for pulling door |
|
6 |
Inspection glass |
14 |
Locking for low-voltage cabinet door |
|
7 |
Opening for manual charging of the circuit-breakers energy storing device |
15 |
Switching EvoPacT HVX-O OFF |
|
8 |
Option for defeating the close door interlock (to be operated only by authorized person) |