VDRB05981-03

Transport

WARNING
HAZARD OF toppling
  • When transporting the switchgear, ensure that the units remain stable and do not tilt or tip over.
  • Nail down the transport pallets to the loading surface.
  • When transporting the trucks, comply with the transport guidelines in the relevant manuals.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
CAUTION
HAZARD OF Equipment toppling
  • For transport, the cubicles must be packaged completely.
  • The entire length of the forks must be placed under the transport unit.
Failure to follow these instructions can result in injury or equipment damage.

Transport with Forklift Truck

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?