VDRB05981-03

Earthing the Busbar

DANGER
hazard of electric shock, explosion, and arc flash
  • Truck (EvoPacT HVX-O VCB and EvoPacT Metering) in the appropriate busbar sections must be in disconnected position.
  • Observe the conditions of Operations and Interlocks.
Failure to follow these instructions will result in death or serious injury.

Earthing the Busbar with Busbar E/S in the Metering Panel

Initial Situation:

  • Busbar earthing switch: OFF

Earthing the Busbar

Switch ON the earthing switch (1).

Earthing the busbar with earthing switch

De-earthing

Switch OFF the earthing switch.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?