VDRB05981-03

Important Information for Assembly

The PIX-36 cubicles are delivered with earthing switch ON position. The VCBs are always shipped in an open state (OFF) with the energy-storing device released.

NOTICE
HAZARD OF NON COMPLIANCE TO ASSEMBLY INSTRUCTIONS
  • Ensure there is no condensation, dirt, and dust during assembly of panels on all accounts.
  • Observe and read assembly drawings before commencing the assembly work.
Failure to follow these instructions can result in equipment damage.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?