VDRB05981-03

Operations

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
  • Maintenance work must only be performed by trained electricians with proven experience of the PIX-36 and all the relevant safety standards.
  • Comply with the operating sequences.
  • Perform every switching operation completely.
  • Ensure the presence of voltage in the system.
  • After each switching operation for which a crank or a lever or a handle is used, remove this tool and store it in the tool board.
Failure to follow these instructions will result in death or serious injury.
CAUTION
hazard of incorrect operation
In case supply voltage is not available:
  • Check if blocking coils (locking the interrogation slides and CB push buttons, depending on design) are in locked position.
  • Check if an under voltage release (optional) has dropped out.
  • Measure: Re-establish the supply voltage.
Failure to follow these instructions can result in injury or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?