VDRB05981-03

Opening and Closing the Front Door

Opening the Front Door

  1. Make sure truck is in disconnected position.

  2. Pull the handle lever.

  3. Rotate the handle clockwise (approximately 120°) to unlock.

  4. Open the front door by pulling the handle.

  5. Access the switching device.

Handle in open condition

Handle in intermediate condition

Closing the Front Door

  1. Close the door completely.

  2. Press the front door slightly to compress the gasket.

  3. Rotate the handle anti-clockwise (approximately 120°) to lock.

  4. Press the handle to rest position.

Handle in close condition

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?