VDRB05981-03

Switching ON the Earthing Switch in case of Solenoid Interlock

NOTICE
hazard of inappropriate operation
Do not insert earth switch handle when slider visible in slot.
Failure to follow these instructions can result in equipment damage.

Initial Situation:

  • Earthing switch: OFF

  • Circuit Breaker: OFF

  • Truck: Disconnected position

Follow the below steps to switch ON the earthing switch in case of solenoid interlock:

  1. Press and hold the push button to gain access.

  2. Rotate the flap anti-clockwise to access the operating shaft.

  3. Insert the operating handle aligned with axis point.

  4. Turn the handle counter-clockwise by 90° to close the earthing switch.

  5. Check the earthing switch position indicator through rear cover and ensure that the earthing switch is OFF.

  6. Remove the earthing switch handle and place it back into the tool board.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?