VDRB05981-03

Rack-in the Truck from Disconnected Position into Service Position

Follow the below steps to rack-in the truck from disconnected/test position into connected/service position:

  1. Move the slider (1) to the left and hold it.

  2. Insert the truck handle (2) through the opening guide in the door onto the drive shaft of the CB truck.

  3. Turn the truck handle (2) clockwise until the truck is racked-in.

  4. Remove the truck handle (2) and place it back into the tool board.

  5. Check the position of the truck through the inspection glass (3).

Truck racked-in service position

Racking-in the Truck via Truck Handle

1

Slider

2

Handle

3

Indicator

NOTE: During the rack-in/rack-out, the door gets locked to help prevent it from opening. The door can be unlocked only if the truck is in the disconnected/test position.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?