Insertion of the Truck into the Cubicle
Initial situation:
-
The VCB is Closed/OFF, discharged and in disconnected/test position.
-
The panel shutters are not padlocked.
Follow the below steps for insertion of the truck into the cubicle:
-
Open the VCB compartment door.
-
Check the compartment for:
-
Cleanliness in accordance with the service conditions.
-
No installation scraps or items have been left inside (tools, electrical wires, broken parts or shreds, metal objects, and so on).
-
-
Position the truck in front of the panel.
-
Align the ramp with the cubicle rails.
-
Slide the truck locking handle inwards.
-
Push the VCB by holding the locking handles, into the VCB cubicle to its test position.
WARNINGhazard of Equipment toppling- Ensure that the pins of the truck is properly aligned to the holes on the panel.
- Move the truck towards the cubicle until the secure lock engages with the panel and firmly arrests it in place.
Failure to follow these instructions can result in death, serious injury, or equipment damage. -
Lock the truck in slots of guide rails by sliding the truck locking handles outwards. Refer to figure 20.
-
Close the VCB compartment door.