VDRB05981-03

Cubicle Variants

The illustrations show the panel types with their respective basic equipment without pressure relief duct or deflectors. Customized models or add-on elements are described in the switchgear-specific documentation.

Branch Circuit Panels with Switching Devices

  • EvoPacT HVX-O VCB

  • Withdrawable Voltage Transformers Optional

  • Earthing Switch (Optional)

Branch Circuit Panels with Switching Devices (Single line)

Metering Panel

  • Metering Truck (MTX)

  • Earthing Switch (Optional)

Metering Panel (Single line)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?