VDRB05981-03

Fastening on Concrete Foundations

Follow the below steps to fasten the cubicle to the floor on standard civil engineering works.

  1. Position the first cubicle on the floor in accordance with the switchgear-specific space assignment plan.

  2. Remove the cable compartment cover.

  3. Once the cubicle is positioned:

    • Verify that the cubicle front is correctly aligned both horizontally and vertically.

    • If necessary, raise the cubicle and insert shims below the cubicle near the fastening points until the correct horizontal position is achieved.

  4. Fasten the cubicle with screws to the two fastening points on both the front end and the rear end.

Fastening of cubicles on concrete foundation

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?