VDRB05981-03

Demounting and Mounting the Cable Compartment Cover

Demounting the Cable Compartment Cover:

  1. Release the securing bolts (1) on the cable compartment cover.

  2. Lift the cover (2), with the help of handles provided, to release it.

  3. Pull the cable compartment cover (3) to remove it.

  4. The cable compartment is now accessible.

Demounting the Cable Compartment Cover

Mounting the Cable Compartment Cover:

  1. Place the cable compartment cover (2) on to the panel, after completing the assembly work.

  2. Fasten it using securing bolts (1).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?