VDRB05981-03

Removal and Insertion of LV Connector

The LV connector can only be removed or inserted while the truck is in its disconnected/test position.

Removal of LV Connector

  1. Pull the interlocking lever of the LV connector forward (1).

  2. Remove the connector (2).

  3. Fix the LV connector to the pin on the EvoPacT HVX-O VCB.

Insertion of LV Connector

  1. Remove the LV connector from the fixation pin on the EvoPacT HVX-O VCB.

  2. Insert the LV connector into the socket of interchangeability interlock inside the cubicle above the EvoPacT HVX-O VCB.

  3. Press the interlocking slide forward.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?