VDRB05981-03

Handling Instructions

WARNING
HAZARD OF EQUIPMENT TOPPLING
  • Wear appropriate PPE.
  • Handle the equipment with appropriate care as specified below.
  • Keep the cubicle in vertical orientation while handling.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The transport and handling information for a cubicle are as follows.

  • The conditions and types of transport have been stipulated in the contract details.

  • The type of packaging depends on the type of transport and the storage conditions.

  • The cubicles are delivered individually and are fastened on pallets. The standard accessories are included.

  • The transport trolley with accessories will be dispatched in a separate box.

  • The EvoPacT HVX-O rated above 2500 A will be dispatched in a separate package.

  • The cubicles are delivered in vertical position.

  • The weight of the entire transport unit is indicated on the packaging.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?